AD698: R3 calculation error in datasheet phase lead phase lag compensation

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

On the AD698 datasheet, page7, Equation (2), When Vos=5V, R4 is open, R2 is
41.7 for VOUT 0~10V
In terms of Equation (2), the R3 should be 8Kohm. But R3 is 7.02Kohm in
datasheet. There is some
mistake on it? ?Figure1?

 

You are correct saying that R3 should have a value of 8 kOhm. This is probably
a mistake in the datasheet.

Outcomes