AD698: Power supply +/-12V

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is it possible to operate the AD698 from a +/- 12 volt supply as it states the
minimum DC dual supply should be +/- 13 V in the data sheet and if so are there
any compromises in the performance of the device apart from a smaller output
swing.

 

Besides the output voltage range, the rest of the data sheet is valid if +/- 12
V supplies are used. Also the Typical Performance Characteristics plots cover a
range of supplies from +/-12 V to +/-18 V.  Ensure that a headroom of 3V is
maintained when designing the output signal.




Attachments

    Outcomes