The advantage or special consideration of using dB output instead of the RMS output of AD637

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the advantage or special consideration of using dB output instead of
the RMS output of AD637

 

The dB feature provides a log conversion of the input voltage such as typically
used by audio sound-level instruments, or other things such as VU meters, etc.
It is a more useful sound or loudness metric than a linear response as it is
capable of displaying a wide dynamic range of audio levels.

Attachments

    Outcomes