AD6624A: In slave mode, can you use DR to drive SDFS input

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

When using serial ports in slave mode is it possible to connect DR to SDFS of
same port to initiate data output? There isn't any info on the time DR is
asserted in datasheet specifications?


In slave mode it is permissible to use DR to drive the SDFS input.  The SDFS
would be recognized on the next clock cycle after the DR goes high and the data
output would begin on the next clock.