AD621 data sheet Rev.B,  SOIC Package (dimension height) error

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

There is a discrepancy data sheet error as reference below, which are not
aligned. can you advise which package is correct.

discrepancy

(a) In wwww.analog.com. Under the AD621 product page for AD621ARZ, under the
section "Price, packaging, availability", and on the 'Package' column wrt SOIC
Model. The package on height dimension was given as 1.75mm

(b) In the AD621 data sheet Rev.B,  SOIC Package (page 16). Max height of the
(SOIC (R-8)is 2.59 mm

Can you advise correction and discrepancy.

 

The AD621 data sheet Rev.B,  SOIC Package (dimension height) of 2.59mm is wrong
and web page of 1.75mm is correct.

We have since migrated all of our SOIC packages to the JEDEC MS-012 standard,
which specifies 1.75mm maximum height. We apologies for this typo error, Author
for this data sheet had been notified and had also been verified. Author will
correct data sheet on next revision.

Attachments

    Outcomes