AD590: How to measure temperature of a steel plate

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I want to use AD590KF to measure the temperature of a piece of steel plate.
Which side(Side 1 or Side 2) should be attached on the steel plate? And how he
attach the AD590KF to the plate?
If I want to test the temperature(about 50 degree)  of the Steel Plate, then
can I place the Side 2 to the Plate, is it Ok?

 

Yes, you should thermally connect side 2 of the package to the steel plate,
using thermal adhesive.

You should also make sure that there is no other heat source sharing the same
GND on the PCB.

Attachments

    Outcomes