AD5750-1: Can the software determine which variant of AD5750 is populated -1 or -2?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can the software determine which variant of AD5750 is populated -1 or -2?

 

What we have characterized is that the reset cycle typically takes 30us, we
can’t guarantee the behavior of the part receiving SPI signals during this
reset cycle time. In other words, we can’t guarantee if the SPI data is clocked
in by the part during the reset cycle.

Attachments

    Outcomes