DEMO-AD5700D2Z kit : Finding a low cost IDE

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I am looking at using the DEMO-AD5700D2Z kit (Complete 4 mA to 20 mA Loop
Powered Field Instrument with HART Interface) and want a low cost development
environment for modifying the sample code provided. Please can you advise which
IDE I should use as the list on your pages doesn't seem to include the M3
products.




 

Any tool supporting SWD and Cortex M3 can be used for the development with our
Cortex M3 products including the ADuCM360 microcontroller used on
DEMO-AD5700D2Z kit

There are several free IDEs that you could use, for example:

emIDE :  www.emide.org/
Eclipse:  www.eclipse.org/

Other useful resources:

ADuCM360 Development system  webpage:

http://www.analog.com/en/processors-dsp/analog-microcontrollers/aducm360/product
s/EVAL-ADUCM360/eb.html

We provide code limited evaluation versions of IAR and Keil with our Cortex M3
based ADuCM360 Developments kits:

http://wwwp.analog.com/en/evaluation/eval-aduc-cable1z/MicroConverter_Developmen
t_Tools/fca.html#cortexM3

Links to IAR and Keil:

http://www.iar.com/
http://www.keil.com/arm/mdk.asp

Attachments

    Outcomes