AD5554: Bias over temperature

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Assuming I use the AD5554 the data sheet is vague about the Vss bias facility.
Is there any additional information available to indicate at what temperature
this facility should be used?

 

The AD5554 is spec'd over -40 to 85 degC. The limits on the spec table is for
VSS=0V. If you are satisfied with the spec, biasing VSS to 0V should be fine.
The output leakage is slightly better when VSS is less than 0V. The FAB process
is well controlled, the difference in Iout leakage between VSS=0V and VSS=-5V
is very small over the temperature range, in the order of a few nA.

Attachments

    Outcomes