AD5554: Current circuit

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

How uses the current output? Because with the application note, the output is
directly converted in voltage and after to current.

My application is very easy, I would like generated a same current into a
variable charge (NTC). Could you help me?

 

The max output current of the DAC is 2.5mA. You can drive any Resistive load ,
but the NTC must be of high value.(>10K)
If not, you have to use some interface circuitry to boost the current, like
that of the application note.

Attachments

    Outcomes