Using toggle mode in the AD5384 using an I2C interface

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I'm running the AD5384 in i2c mode, and would like to know 2 things:

1: Is it possible to use toggle mode in i2c interface mode?  The final
paragraph in 2 Byte mode states "toggle mode is not supported in 2-byte mode". 
This implies that toggle mode is supported in 3 and 4 byte i2c modes.

2: If toggle mode is supported in i2c mode, how do I write to the a and b
registers?  Table 20 in the documentation shows a bit that determines whether
register A, or B are being written to.  Where/how is the corresponding bit set
in the i2c interface?

 

This looks like an oversight in the datasheet. Toggle mode is possible in I2C
mode. The MSB of the pointer byte is the A/B bit. Figure 34 of the AD5390
datasheet shows this clearly (relevant for AD5384).

Attachments

    Outcomes