Does AD5245 (Potentiometer) have a log or linear taper?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is the AD5245's taper logarithmic or linear?

We need the taper to be logarithmic, as we will use it in Volume Control

 

The AD5245's taper is linear. We do not have logarithmic taper potentiometers.

The following Circuit Note (CN0120) shows logarithmic Audio Volume using the
AD5292 potentiometer:
http://www.analog.com/en/circuits-from-the-lab/CN0120/vc.html

Attachments

    Outcomes