AD5243 VOL output logic level

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 3Show Document
  • View in full screen mode

I am searching for the Vol (output low voltage level) as the I²C pins are also
open-collector outputs! What's the value for Vol?

 

Based on the simulations for a worst case conditions, the max Vol is around
80mV for 4mA sink. (see attached)

Outcomes