AD5115 Digipot

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I have one technical question regarding the digipot AD5115 we are currently
using:
1. Wwhat is the default value in the EEPROM of the device after the
manufacturing? MIN, MAX/2, MAX or undefined value?
2. Can we use this value in production, without writing the EEPROM? or it is
not recommended?

 

This info needs to be in the DS, similar to the AD5110.EEPROM is pre-loaded to
midscale at the factory, and initial power-up is, accordingly, at midscale.

We’ll add this info  asap.

Attachments

    Outcomes