AD2S80A: Can 2 AD2S80As be used with the same inductosyn?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can 2 AD2S80As be used with the same inductosyn?

 

Yes, but they must have the same reference frequency from the same excitation
source.
I don't see any problem in principle with connecting two AD2S80A components to
the same output. Both devices have an input buffer so they shouldn't load the
pre amp output. I assume that both outputs will receive the same reference
frequency from the excitation source.

Attachments

    Outcomes