data sheet error. Hold time of A0 and A1 signal during SPI transfert on AD2S1210

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

T33, The hold time for A0, A1 do not seem to be correct or aligned to the
parameters.

 

It should be related to SPI clock and not the CLKIN frequency.

A0 and A1 should hold their value for the duration of the data read and after
that they can be released or set to a new state.

Upon review and analysis wrt AD2S1210 datasheet.  There appears to have typo
errors in the timing parameters. Have liaison with the author for this
datasheet.

The hold time for A0, A1 should be related to SPI
clock and not the CLKIN frequency. Currently the datasheet is being revise to
include these changes. Please see attached temporary cut down version for the
time
being.

Attachments

    Outcomes