AD2S1200: Can AD2S1200 be used with "SINCOS" sensor?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can AD2S1200 be used with "SINCOS" sensor?


Yes, if by "SINCOS" sensor you mean a Resolver (resolver is like a
motor/generator with windings at 90 degrees so it gives Sin/Cos outputs).
The converter accepts 3.6Vp-p ±10% input signals, centered around 2.5V, in the
range 10 kHz 20 kHz on the Sin and Cos inputs. A Type II servo loop is employed
to track the inputs and convert the input Sin and Cos information into a
digital representation of the input angle and velocity”