AD2S1200: The full scale value for the velocity output is not given in datasheet

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I can not find the full scale value for the velocity output in the AD2S1200
datasheet.

 

The velocity output of the AD2S1200 is in twos complement format and is scaled
to a maximum velocity of +/-1,000rps [60,000rpm] i.e. when reading back
velocity 800h will represent -1,000rps and 7FFh will represent +1,000rps. Each
bit is equivalent to 1000rps / 2048 i.e. 0.488rps.

Attachments

    Outcomes