Datasheet for AD22290

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Customer have an accelerometer from Analog which is marked with no. 22290 & he
is not being able to find it's datasheet anywhere on the net.

It's dimensions & pin positions are same as of AD22282/83/86.  whether it is
1/2/3 axis accelerometer or it's pinouts & whether they are different from
AD22282/83/86.

 

The AD22290 is an obsolete special based on the ADXL311 (pretty old). It is
specified as a 2 axis analog output accelerometer with 3V supply voltage. You
can look at the ADXL311 data sheet for pin out, etc.

Attachments

    Outcomes