What is a power consumption of AD2S1200?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

In data Sheet it states only: "POWER SUPPLY IDD Dynamic 18 mA", but for the
power budget I need to know the worst case. Can you provide separate values for
AVDD and DVDD (both 5V). The Load on EXC/bEXC is around 5k


IDVDD and IAVDD are both max at 10 mA. The EXC load shouldn't really matter as
the EXC output cannot be used to drive resolver directly therefore buffer
circuitry is needed.