AD215: do you have tests available against EN60335-1

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

For AD215, I would like to know if you have performed the test of electric
strength in
agreement with the EN 60335-1 (par 16.3) the insulation is subjected to
a voltage having a frequency of 50 Hz or 60 Hz for 1 min [...].
The values of the test voltage for different types of insulation are given in
Table [..]
1800Vrms is intended for the electric strength test?

 

This is an early 1990’s vintage product and we do not have any EN 60335-1 test
data.

So far there are NO plans to to test according the EN 60335-1.

Isolation Amplifier have been widly used 20 years ago. The technology has been
replaced by digital Iso-Couplers - Isolation is on the digital side compared to
Isolation on the analog side.

Attachments

    Outcomes