output short circuit

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Could you email me the amplifier output short circuit (not the power supply)
specifications, Iout max?, type of load for this device? Etc. There is nothing
on the data sheet.

 

The only specification we have specifically relating to the output current is
that the AD210 module can swing its full +/-10V range with a 2K resistive load
applied and the Isolated power supplies are not fully loaded.
Beyond that I can only mention that the output amplifier is currently an
ADTL082 and although the output amplifier could change in the future, this is
the type of amplifier we would typically use for the output amplifier.

Attachments

    Outcomes