The relationship between value of Input Level Control register (Address 0) and gain value

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the relationship between value of Input Level Control register (Address
0) and gain value? Why 1.8836 is corresponding to the gain of 11dB?

 

A gain of G=1.8836 corresponds to 5.5dB and in the AD1970, this value is
multiplied by 2 to get a level of 11dB. Thus, a gain of 1.99 – the maximum
allowed by the binary format here – would yield a gain of ~12dB (11.95dB).

Attachments

    Outcomes