AD1852: ESD sensitivity, HBM model data missing from datasheet

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I couldn't find in datasheet the parameter called Human Body Model which
informs me about ESD sensitivity of IC. In data sheets for most other
components, HBM parameter appears in Absolute Maximum Ratings list. Could you
let me know what is HBM value for the AD1852?

 

Here is the test data that I found for this device:

ESD Model : HBM
Class: 3
ESD Test Spec used: ESD Association S5.1
RC network: 1500 ohm, 100pF
Highest Pass: 4500V
First Fail Level: 5000V

Attachments

    Outcomes