FAQ: Installation tips for best results with BLIP board

Document created by npai2 Employee on Dec 7, 2015Last modified by NagarjunaG on Jan 8, 2016
Version 2Show Document
  • View in full screen mode

The BLIP board has 2 on board sensors - The OVM7692 and ASX340AT sensors. For best results the use of ASX340AT is recommended. Choose any of the two on board sensors and install it such that the correct sensor faces the scene. The sensor must be aligned to the field of view (FOV). The imaging sensor must be facing at an angle towards the field of view (perspective installation) or directly facing downwards at zero degree angle (direct overhead installation).

 

For an perspective installation, the BLIP board must be mounted at a height of 25-40 ft to get a FOV (Field of View) of at least 90 degrees. The sensor then covers a FOV of 20-30 ft diameter of the scene being monitored.

 

The FOV of the installation for our testing is shown below:

temp.png

 

This FAQ was generated from the following discussion: Setup/installation of the BLIP board?

Attachments

    Outcomes