FAQ: What operating systems are supported to run SigmaStudio?

Document created by JeradL on Jan 21, 2010Last modified by JeradL on Dec 23, 2010
Version 4Show Document
  • View in full screen mode

At this time, the fully supported operating systems are Windows XP, Windows Vista, and Windows 7. SigmaStudio 3.3 is the first version that includes full support for Windows 7 and is available in both an x86 (32-bit) and x64 (64-bit) version. The download file includes both installers; please choose the appropriate one for your PC.


This FAQ was generated from the following thread: How can Sigma Studio 3.1 run under Windows 7?