Output drive current for ADA4661-2 and ADA4666-2

Document created by MH@CAC Employee on Nov 10, 2015
Version 1Show Document
  • View in full screen mode

Q:

How high of an output current can the ADA4661-2 and ADA4666-2 drive?

 

A:

 

The ADA4661-2 and ADA4666-2 are capable of driving output currents up to 30 mA with only 1V of dropout voltage. However, the usable output load current drive is limited to the maximum power dissipation allowed by the device package used. Always make sure not to exceed the maximum junction temperature (150C) of the device. To ensure proper operation, observe the following graph:

 

Attachments

    Outcomes