Advantiv™ Video Evaluation Software (AVESBlue)

Document created by GuenterL Employee on Oct 16, 2015Last modified by GuenterL Employee on Jul 24, 2017
Version 18Show Document
  • View in full screen mode

Advantiv™ Video Evaluation Software AvesBlue

 

This version of AVES is an upgraded version of AVES3 with the intent to eventually replace AVES3 and all previous versions

 

New features:

  • Improved User Interface
  • Integration of IronPython 2.7
  • I2C plug-in drivers, allows user to create their own interface to the target
  • Handles multiple instances of same chip type on a single board

 

ChangeLog:

  • 3.03.0627 - October 16, 2015
    • Initial release
  • 3.03.0656 - October 19, 2015
    • Project folder must not have space in its name, added warning box when re-configuring display
    • Re-configure display now displays all the tab, not just checked tabs
  • 3.03.0700 - October 21, 2015
    • Now handles project folder names with spaces in them
    • Added File->Reset Tab Sequence to return tabs to configured order
    • Closing floating project tabs will put tab back in main window in the correct sequence
    • Added Preference->Enable Short Cut Keys checkbox
  • 3.03.0906 - November 6, 2015
    • Fixed the broken Settings -> Configure Display
  • 3.03.1030 - March 10, 2016
    • Completed Bus Configuration to handle multiple instances of the same device
    • Updated Probe for new Bus Configurator
    • Included UBoot driver
    • Updated documentation
  • 3.03.1243 - April 18, 2016
    • Enhanced Meta-Field editor window, changed to multiple opened non-model windows with dynamic updates
    • Removed draggable tabs feature
  • 3.03.1254 - May 4, 2016
    • Fixed issue with UBoot driver
  • 3.03.1536 - Oct 3, 2016
    • Added HSF2 driver for ADI HDMI Software Framework 2.0, ADV7664 eval. board
  • 3.03.1545 - Jan 13, 2017
    • Tweak to HSF2 driver for better access to ADV7664 board
    • Minor tweak to core code
  • 3.03.1557 - April 5, 2017
    • IronPython path configuration expanded to 20 entries
    • Removed UBoot driver.
    • Changed HSF2 driver to 921000 kBaud
  • 3.03.1558 - July 24, 2017
    • User guide update
7 people found this helpful

Outcomes