FAQ: How to handle different types of sensors used in WSN solution?

Document created by NagarjunaG Employee on Jul 27, 2015Last modified by NagarjunaG Employee on Jul 27, 2015
Version 2Show Document
  • View in full screen mode

This is applicable to both ADWSN solutions (ADRadioNet and AD6LoWPAN). 


The specific sensor values that are being sent from a given sensor mote can be determined by the "sensor mask" value. This value is part of the payload sent from the node. The feature of sensor mask is added in the ADRadioNet EDKv2.0 & AD6LoWPAN EDKv1.0. Users can download the latest code from the download link from  EngineerZone pages (ADRadioNet and AD6LoWPAN), or, directly from http://www.analog.com/wsn

 

The two byte "sensor mask" is as shown below.

sensor_mask.png

In both ADRadioNet & AD6LoWPAN, the above "sensor mask" is assumed. If some sensors are to enabled in a specific node, those alone will be enabled in the sensor mask register. The sensor data corresponding to these enabled sensors will be available in the prescribed order as defined by the user (from LSB side). The length of the each sensor payload is defined a priori (for example, the accelerometer sensor will have 3 float values corresponding to x, y & z-axis. Similarly, for ALS, it is a single value. All values are assumed "float" for ease of implementation).

 

Please find the example sensor information packet below, captured by the PC UI tool, by enabling the following sensors

  • ADT75 ==> Temperature
  • ADXL362 ==> Accelerometer
  • SHT21 ==> Temperature and Relative Humidity
  • ALS   ==> Ambient Light Sensor APDS9005

AD6L-ADRN-Packets.png

The sensor data is color coded in this example as below. The statistics information is available right after the sensor data.

Yellow color ==> INT_MARK     

Light Green  ==> SINGLE_MARK 

Red color     ==> Sensor Enable Mask

Dark Green   ==> Temperature Data

Dark Yellow ==> Accelerometer (X, Y and Z axis)

Grey color   ==> Temperature and Relative Humidity

Pink color    ==> Ambient Light Sensor APDS9005


In this example, the sensor mask = 0x0056, indicating the following sensors are enabled in the system - ADT75, ADXL362, SHT21 and ALS (APDS9005). The below table shows how the value of mask is calculated.

sensor_mask_example.png

The sensor data representation corresponding to this example, at “Network overview” window of PC tool will be as below

 

Sensor Data

FLOAT[0]

ADT75 Temperature

FLOAT[1]

ADXL362 X-axis

FLOAT[2]

ADXL362 Y-axis

FLOAT[3]

ADXL362 Z-axis

FLOAT[4]

SHT21 Temperature

FLOAT[5]

SHT21 Relative Humidity

FLOAT[6]

ALS (APDS9005)

 

Please note, the overall schema of this sensor representation can be changed based on user requirement. (like for example - the easiest is changing the sensor mask register as per user requirement; for this few modifications in code are required). It is up to the user to add an application level logic to handle the sensor data as desired.


This FAQ was generated from the following discussion: Identifying sensors enabled and sensors data, from a data packet of WSN node in a network.

1 person found this helpful

Attachments

    Outcomes