FAQ: Operating Modes & Supported data rates in AD6LoWPAN

Document created by NagarjunaG Employee on Jun 24, 2015
Version 1Show Document
  • View in full screen mode

The following table shows the operating modes, corresponding data rates and number of channels that are supported in AD6LoWPAN solution.


The maximum data rate that is supported currently is 100kbps. The frequency bands and the data rates are according to IEEE 802.15.4g specification.


The user does not have the control to modify these values as these are configured internally based on the frequency band and the PHY_MODE selected by the user from the ADWSN-UI-Tool.

 

S.No

ISM Band
Supported

Operating
Mode & Data Rate

Number of Channels

1

863–870
(Europe)

Mode 1  50 kbps  2FSK

17

Mode 2  100 kbps  2FSK

17

2

896–901
(U.S. FCC Part 90)

Mode 1  10 kbps  2FSK

255

Mode 2  20 kbps  2FSK

255

Mode 3  40 kbps  2FSK

255

3

901–902
(U.S. FCC Part 24)

Mode 1  10 kbps  2FSK

73

Mode 2  20 kbps  2FSK

73

Mode 3  40 kbps  2FSK

73

4

902–928 (U.S. ISM)

Mode 1  50 kbps  2FSK

64

5

917–923.5 (Korea)

Mode 1  50 kbps  2FSK

32

6

928–960b
(U.S. FCC Part 22/24/90/101)

Mode 1  10 kbps  2FSK

255

Mode 2  20 kbps  2FSK

255

Mode 3  40 kbps  2FSK

255

7

920-928 (Japan)

Mode 1  50 kbps  2FSK

18

Mode 2  100 kbps  2FSK

18

8

950-958 (Japan)

Mode 1  50 kbps  2FSK

16

Mode 2  100 kbps  2FSK

16

 

This FAQ was generated from the following discussion: What data rates are supported in AD6LoWPAN and what is the maximum data rate supported?

Attachments

    Outcomes