FAQ:  How to boot the BF537?

Document created by EJR on Dec 11, 2009Last modified by AndyR on May 19, 2011
Version 4Show Document
  • View in full screen mode

Q:

How do I boot the Blackfin Processor BF537 from 16-bit flash memory?

 

----------

 

A: 

EE-240 is an excellent reference for booting questions.  It was written for BF533, BF532 and BF531 but the process also applies to the BF537 and other Blackfin parts.  It shows that either an 8 or 16 bit flash can be used.  Simply specify the memory type when creating a loader (.LDR) file.

 

----------

 

 

 

This FAQ was generated from the following thread: How to boot the BF537?

Attachments

    Outcomes