Can I use the MLB Clock on SC58x to clock an external system?

Document created by vinodbableshwar on Jun 12, 2015
Version 1Show Document
  • View in full screen mode

The MLB clock signal is available as part of the pin mux. Pin PD14 when configured with the MUX configured as “10” will route the MLB clock on this pin which can be used for external connections.