ADSP-SC58x/2158x SPDIF-RX feature list: What's new?

Document created by SachinV Employee on Jun 10, 2015Last modified by SachinV Employee on Jun 10, 2015
Version 2Show Document
  • View in full screen mode

The ADSP-SC58x/2158x processors have new SPDIF receiver design. The features are:


1. It supports sampling rates from 24KHZ to 96KHZ

2. It can detect Audio word length from channel status bits as specified by IEC 60958-3

3. It can detect compression type by using burst info as specified by IEC 61937-2

4. It can detect whether compression type is DTS or AC3.

5. It doesn't support interrupt for CRC error and parity error and emphasized audio( These are supported in ADSP-214xx).

6.The SCDF mode which was supported in ADSP-214xx is not available in new design

1 person found this helpful