ADAS3023 - power supply sequencing

Document created by KarenNE Employee on Mar 16, 2015
Version 1Show Document
  • View in full screen mode

Q: What is the correct power supply sequence for the ADAS3023 to operate properly?

 

A: The ADAS3023 requires these five supplies: AVDD = +5V, DVDD = + 5V, VDDH = + 15V, VSSH = - 15V, and VIO = 1.8V to 5V. The user must bring up the ADAS3023 power supplies in the following sequence in order to operate it normally:

1. VIO

2. VDDH

3. VSSH

4. DVDD

5. AVDD

6. REFx

 

In order to operate the ADAS3023 from a + 5V single supply, the user would need to generate the required +/-15V high voltage supplies using one of our switching converters such as the ADP1613/14 in SEPIC-Cuk topology. Refer to CN-201 for complete information on this test setup.

1 person found this helpful

Attachments

    Outcomes