What is the highest RF output frequency supported by the AD9144?

Document created by YiZ on Nov 12, 2014
Version 1Show Document
  • View in full screen mode

The AD9144 has an on-chip NCO that can be used to modulate quadrature input signals up to half the Nyquist rate of the DAC.  When running at the maximum DAC update rate of 2.8GSPS this allows customers to output frequencies up to 1.4GHz.

1 person found this helpful

Attachments

    Outcomes