AD9135/AD9136 - How do I select between the two parts?

Document created by rdowning on Nov 6, 2014
Version 1Show Document
  • View in full screen mode

The AD9135 and AD9136 are two product variants in the same product family. The only difference is the DAC resolution. The AD9135 is an 11-bit dual DAC while the AD9136 is 16-bit. All the other features and specifications are exactly the same in the two products. The AD9135 is suitable for the applications that do not need a full 16-bit resolution.


For more information, visit the product pages


AD9135

AD9136


Attachments

    Outcomes