AD936x Built in Self Test (BIST)

Document created by tlili Employee on Oct 15, 2014Last modified by tlili Employee on Oct 20, 2014
Version 2Show Document
  • View in full screen mode

BIST Signal Generator

 

AD9361 and AD9364 have an internal signal generator which can be used to inject a signal into either the output of the Tx data port or the input of the Rx data port. This is useful when testing the connectivity of the Rx data port or the Tx RF output. It is a useful tool when debugging effects in the Tx chain of the AD9361. It allows the user to rule out the Tx data port as the source of issues, as it allows the user to generate a signal and inject it at the output of the Tx data port. Please see the attached document for more details.

14 people found this helpful

Attachments

Outcomes