µC/OS-II, µC/OS-III, µC/FS and µC/USB Device Stack 1.1.0 – Available Now

Document created by ColinJ on Aug 13, 2014Last modified by ColinJ on Aug 14, 2014
Version 3Show Document
  • View in full screen mode

The latest release of the µC/OS-II, µC/OS-III, µC/FS and µC/USB Device Stack (1.1.0) for CrossCore Embedded Studio are now available and can be downloaded from their respective Product Pages:-


µC/OS-II Real-Time Kernel product page

µC/OS-III Real-Time Kernel product page

µC/FS Fie System product page

µC/USB Device Stack product page


Further details of whats new in each release are detailed in the 1.1.0 release note for each Add-In - available from the Product Page.

 

The µC/USB Device Stack (1.1.0) release introduces support for the ASDP-BF70x, ADSP-BF518 and ADSP-214xx processor families and also includes the following collection of uC/USB Device add-in products for CrossCore Embedded Studio:


µC/USB Device Core for CrossCore® Embedded Studio

µC/USB Device Class CDC-ACM for CrossCore® Embedded Studio

µC/USB Device Class HID for CrossCore® Embedded Studio

µC/USB Device Class MSC for CrossCore® Embedded Studio

µC/USB Device Class PHDC for CrossCore® Embedded Studio

µC/USB Device Class Vendor for CrossCore® Embedded Studio

 

Note that it also includes the following New Class:


µC/USB Device Class Audio for CrossCore® Embedded Studio

 

For details of what’s new in this 1.1.0 release, please refer to the uC/USB Device Stack for CrossCore Embedded Studio Release Note.

 

All µC/USB Device add-in products have been updated to use the 4.02.00 release of the Micrium uC/USB Device StackSee Micrium’s release notes for further details.



The following Board Support Package (BSP's) have also been updated to release 1.1.0:


Audio EI3 Extender Board

Blackfin SHARC USB Extender Board

Camera EI3 Extender Board

Blackfin USB-LAN Extender Board

Video Decoder EI3 Extender Board

Video Encoder EI3 Extender Board

WVGA/LCD EI3 Extender Board


Further details of whats new in each BSP are detailed in the 1.1.0 release note - available from the Product Page.



Attachments

    Outcomes