FAQ: Highlights of MSI on BF70x

Document created by Nabeel Employee on Jun 12, 2014Last modified by LindaJ on Jun 23, 2014
Version 2Show Document
  • View in full screen mode

Following are the highlights of Mobile Storage Interface Module on BF70x processors:

  • MSI has an integrated DMA controller to transfer data between the  FIFO and system memory
  • Core accesses to MSI FIFO are not supported
  • Supports Secure Digital memory protocol (version 3.0), • Supports Secure Digital I/O protocol (version 3.0),  Multimedia Card protocol (MMC - version 4.41, eMMC 4.5)
  • Support for automatically generating the STOP command after data transfer(MULTI-BLOCK or STREAM) is finished
  • Flexible FIFO and card threshold controls
  • MMC boot mode support


This FAQ was generated from the following discussion: Highlights of MSI on BF70x