FAQ – Can’t connect to target via emulator after upgrading to CCES 1.1.0

Document created by LindaJ on Jun 11, 2014Last modified by ErinH on Sep 14, 2016
Version 2Show Document
  • View in full screen mode

Q.

After upgrading to CrossCore Embedded Studio 1.1.0, I can no longer connect to my target board using my ICE-100B or SADA 2 emulator. What’s changed?

 

----------------------------


A.

CCES 1.1.0 introduces a new driver for the ICE-100B and SADA 2 products.

 

In order for the Device Manager to correctly identify these emulator products and install the new driver, modifications to the emulator jumper settings need to be made, details of which can be found below. Should you wish to work with earlier version of CCES in future, you will need to reverse these jumper modifications.

 

ICE-100B

 

  • To use the ICE-100B with CCES 1.1.0 and later versions,  JP2 should be populated (ON)

 

When JP2 is ON, the ICE-100B should appear in the Device Manager under ‘CrossCore Tools’.

 

Refer to the following diagram for the location and proper placement of JP2, highlighted in red:

 

1000.jpg

 

If JP2 is OFF and connection to a target is attempted with CCES 1.1.0 or later version, the following error will be reported:

 

Error: 0x8004881f

Error Description: Emulator not supported, JP2 may not be installed

 

 

  • To use the ICE-100B with CCES 1.0.x or VisualDSP++, JP2 should NOT be populated (OFF)

 

When JP2 is OFF, the ICE-100B should appear in the Device Manager under ‘ADI Development Tools’.

 

If JP2 is ON and connection to a target is attempted using CCES 1.0.x or VisualDSP++, the following error will be reported:

 

Error: 0x80048047

Error Description: Failed to initialize emulator

 

 

NOTE: When installing or removing the jumper, the USB cable should be disconnected from the emulator, or unplugged and plugged in again after the jumper has been changed.

 

 

 

Standalone Debug Agent 2 (SADA 2)

 

  • To use the SADA 2 with CCES 1.1.0 and later versions, pins 1&2 of JP1 should be populated (ON)

 

Refer to the following diagram for the location of pins 1&2 of JP1, highlighted in red:

 

SADA2.png 

 

 

When pins 1&2 of JP1 are populated the SADA 2 should appear in the Device Manager under ‘CrossCore Tools’.

 

If pins 1&2 of JP1 are NOT populated, and connection to a target is attempted with CCES 1.1.0 or later version, the following error will be reported:

 

Error: 0xffffffff

Error Description:

 

 

  • To use the SADA 2 with CCES 1.0.x or VisualDSP++, pins 1&2 of JP1 should NOT be populated (OFF)

 

When 1&2 of JP1 are NOT populated, the SADA 2 should appear in the Device Manager under ‘ADI Development Tools’.

 

If 1&2 of JP1 are populated, and connection to a target is attempted with CCES 1.0.x or VisualDSP++, the following error will be reported:

 

Error: 0x80048015

Error Description: Initialization: Open Device Failed

 

 

NOTE: When installing or removing the jumper, the USB cable should be disconnected from the emulator, or unplugged and plugged in again after the jumper has been changed.

4 people found this helpful

Attachments

    Outcomes