CrossCore Embedded Studio 1.1.0 - Available Now

Document created by CraigG on Jun 11, 2014Last modified by ColinJ on Jun 18, 2014
Version 2Show Document
  • View in full screen mode

The latest release of the CrossCore Embedded Studio tools - 1.1.0 - is available now, and can be downloaded from the CrossCore Embedded Studio product page.

 

This release introduces support for the ADSP-BF70x processor family, including build tools support, fast functional Blackfin+ core simulator, debug support and System Services & Device Drivers libraries.

 

It also introduces support for the new ICE-1000 and ICE-2000 JTAG emulators. For more information on these products, see the following link:

Introducing the ADZS-ICE-1000 and ADZS-ICE-2000 Emulators

 

For more information please refer to the Release Note, which is available on the CrossCore Embedded Studio product page, and to get started with the BF70x and CrossCore Embedded Studio, please see Getting Started with ADSP-BF70x Processors.

 

Note: An active CrossCore Embedded Studio Subscription is required to use the latest tools. For more information on License Subscription and Expiration, see the FAQ on the EngineerZone, and the CrossCore Embedded Studio Licensing Guide.

http://www.analog.com/crosscorelicensingguide

Attachments

    Outcomes