Advantiv™ EVAL-ADV8005-SMZ Video Evaluation Board

Document created by mattp Employee on May 22, 2014Last modified by JeyasudhaMuthuPerumal on Feb 18, 2017
Version 18Show Document
  • View in full screen mode

This FAQ applies to EVAL-ADV8005-SMZ.  All support files in their latest versions will be attached below.


Below are the support files for these evaluation board. We recommend that, if you download and use these files, you subscribe to email notifications for either the entire forum or at least this FAQ by clicking on the menu to the right.  In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.


EVAL-ADV8005-SMZ_User_Guide_RevPrB_20140606.pdfPreliminary User Guide for the EVAL-ADV8005-SMZ evaluation board
EVAL-ADV8003-SMZ_rev0p2_schems_20150116.pdfSchematics (in PDF format) for this evaluation board
EVAL-ADV8005-SMZ_BOM_20140911.pdfBOM for this evaluation board

Schematics (in OrCAD format) for this evaluation board

Firmware 1.91.1 for the EVAL-ADV8005-SMZ. You will need to program both the application binary (BF_7625_8005_VSP_1.91RC1_20160526.bin) and the the OSD binary (OSD_1.90SP1_20151125.bin) in order for this firmware to work correctly.

EVAL-ADV8003-SMZ_rev0p2_layout_Allegro_20140630.zipLayout (in Allegro format) for this evaluation board
EVAL-ADV8005-SMZ_20140703.zipAVES3 folder for the EVAL-ADV8005-SMZ evaluation board
FAQ: How can I restore u-boot on EVAL-ADV8005-SMZ?This page explains the hardware/software that is required and process to follow in order to restore u-boot in case it is accidentally deleted.
BF_800x_System_Commands_20150312.pdfList of commands for the current release of firmware for this evaluation board.
EVAL-ADV8003-SMZ_FPGA_files_20130325.zipSource files for the FPGA on this evaluation board.
Software package source code for eval boardDownload HPM software package for AD8005 evaluation board here.


For software documents, go to ADV8005 evaluation board software package documents

Visual DSP Project This is Visual DSP Project file for BF524_7625_8005_VSP_1.91RC1_20160526 software. The software folder is just empty. You can paste the software under 800X_BF_SW folder inside the VDSP project file. Please refer documentADV8005 evaluation board software package documents Advantiv_VSP_Application_ReferencePr0.5.pdf Appendix for the guidelines to compile the VDSP project