How Do I Use an External Oscillator to Clock the ADV728x ?

Document created by Rob.Analog on May 21, 2014Last modified by Rob.Analog on Jan 29, 2015
Version 2Show Document
  • View in full screen mode

In this FAQ the ADV728x refers to the ADV7280, ADV7280-M, ADV7281, ADV7281-M, ADV7281-MA, ADV7282, ADV7282-M and ADV7283 models.

 

Oscillator Specifications:

Firstly you must use an oscillator with an output less than 1.8Vpp. The oscillator must output a 28.63636 MHz clock with a tolerance of +/- 50ppm.

 

Physical setup:

Connect the output of the clock oscillator to the XTALN pin of the ADV728x. Leave the XTALP pin of the ADV728x floating.

 

Software write:

 

The ADV728x normally drives a voltage out on the XTALN and XTALP pins. This voltage is used to power the external crystal. However if a clock oscillator is used instead of a crystal, then this voltage on the XTAL pins can affect the oscillator performance.

 

To prevent this you should perform the following I2C write. Write 0x04 to register 0x13 in the User Map. This write sets the  XTAL_TTL_SEL bit to 1.


  • XTAL_TTL_SEL( User Map, Register 0x13, Bit[2])

When XTAL_TTL_SEL bit is set to 0 (default)  the ADV728x will drive out 1.8 V on its XTALN and XTALP pins.

When XTAL_TTL_SEL bit is set to 1 the ADV728x will not drive out a voltage on its XTALN and XTALP pins.

 

The ADV728x documentation states that register 0x13 is a read only register (status register 3). Actually two registers share the register address 0x13.

When you read from register 0x13, you read back the Status Register 3 data ( this is read only) . When you write to register 0x13 you write to an internal control register. The internal control register is write only and contains the XTAL_TTL_SEL bit .

Attachments

    Outcomes