Getting Started with ADSP-BF70x Processors

Document created by LindaJ on Apr 2, 2014Last modified by mkokaly on Nov 22, 2017
Version 13Show Document
  • View in full screen mode

Getting Started with ADSP-BF70x Processors


ADSP-BF70x Processors


The ADSP-BF70x Blackfin processor series is a high-performance DSP family that delivers a class-leading  800 MMACS of processing power at less than 100mW. The cost-effective eight-member series includes up to 1MB of internal SRAM, eliminating external memory in many applications, while a second configuration features an optional DDR memory interface. Using the enhanced Blackfin+ core, the combination of performance, power efficiency, memory integration, security, and value allows designers to incorporate advanced 16- and 32-bit processing into a range of new use cases, including industrial imaging and building controls as well as portable and automotive audio. The ADSP-BF70x series offers designers unparalleled flexibility and functionality through an array of advanced connectivity options (including USB, SDIO, CAN, ePPI, SPORT, QuadSPI) while enabling bus-powered applications and extending the life of battery-powered devices.


You can learn more about our latest Blackfin processor family on our ADSP-BF70x series product page.

What is required in order to evaluate the ADSP-BF70x Processors?


CrossCore® Embedded Studio (CCES) is a world-class integrated development environment (IDE) for the Analog Devices Blackfin® and SHARC® processor families.  This Eclipse™ based, highly visual IDE enables seamless, intuitive code generation and debug support.  A highly integrated IDE, CrossCore® Embedded Studio is optimized for popular Micrium add-in components including real time operating systems (RTOS), USB and file system stacks. There is also integrated support for a TCP/IP stack. The IDE is combined with Analog Devices advanced optimizing compiler technology and supports standards such as ISO/IEC C and C++, MISRA-C, Embedded C and MCAPI, plus additional development features to get your product to market even sooner.


Further information can be found on the CCES product page and the Getting Started with CCES guide.



The ADSP-BF70x evaluation hardware provides a low cost hardware solution for users to evaluate the Analog Devices ADSP-BF70x processor family.



ADSP-BF707 EZ-Board

CE-approved power supply

ADZS-ICE-1000 emulator

USB A to micro B cable

USB micro A to A receptacle cable

Standoffs and screws

2GB SD card

Release Note


    • The ADSP-BF707 EZ-Board can also be purchased separately, if an ICE-1000 or ICE-2000 emulator is already available to the user.


The ADSP-BF707 EZ-Board Design Database contains all of the electronic information required for the design, layout, fabrication and assembly of the ADSP-BF707 EZ-Board, and is available to download from the Product Downloads area.



The ADSP-BF707 Board Support Package is free to download and use, and does not require a separate license to be installed in CCES.  It provides comprehensive software support for the ADSP-BF707 EZ-Board. Specifically, drivers, examples and code sketches are included for the following components:

    • INA230 current-shunt and power monitor ADC driver
    • INA3221 shunt and bus voltage monitor ADC driver


It also provides comprehensive examples which demonstrate the on-chip drivers and services. 


NOTE: A fast functional simulator supporting ADSP-BF70x processors is also available as part of CCES, details of which can be found here.



How do I begin evaluating the ADSP-BF70x Processors?



When starting CCES for the first time, you will be prompted to install a license. Click ‘Yes’ to install a license and then, in the “Select License Type” window:


    • to begin a 90 day evaluation of CCES, select ‘I do not have a serial number and would like to evaluate the product, and in the “Select license activation method’ window select ‘Install and activate a license on-line all in one step’. Upon clicking ‘Finish’, your evaluation license will be activated and your 90 day evaluation period will begin.


For further information on installing a license see the following FAQ:

How can I obtain and install evaluation and full licenses for CrossCore Embedded Studio?


  • Purchase the ADSP-BF707 EZ-KIT Lite or EZ-Board
  • Install the ADSP-BF707 EZ-Board Support Package.


NOTE: A fast functional simulator supporting ADSP-BF70x processors is also available as part of CrossCore Embedded Studio. Simulation is supported for the following components:

    • Instruction set and core machine state
      • excludes pipeline, cache, and branch predictor
    • Core event controller
    • Internal and external memory spaces
    • Utility ROM images in L2 ROM space
    • Core timer


Addition system components and peripherals will be supported in the simulator in future releases. More information can be found here.



What other development tools and software available for the ADSP-BF70x Processors?


  • Middleware

The following products, which support the ADSP-BF70x family of processors, are available:


  • Algorithmic Software Modules

Free software modules for the ADSP-BF70x family include image processing applications software (such as video occupancy sensing, image processing toolbox, 2D graphics); video imaging codecs such as JPEG and H.264BP/MP; audio codecs including MP3 and ACC; and post processing software including asynchronous sample rate converters and multi-band graphic equalizers.


More information on Blackfin software modules can be found here.


  • Emulators

The newly released low-cost ICE-1000 and high performance ICE-2000 in-circuit emulators support the ADSP-BF70x processor family. Working in tandem with the CrossCore Embedded Studio development environment, these emulators provide state-of-the-art support for all JTAG-compliant Analog Devices processors, which includes program trace, system trace and cross-trigger channel control via Coresight serial wire debug support.


Further information can be found in the Introducing the ICE-1000 and ICE-2000 FAQ.


  • EZ-Extender Boards

EZ-Extender Boards enable developers to connect various peripherals from Analog Devices and from third parties to the expansion interface of the EZ-KIT Lite evaluation kits. The following EZ-Extender boards are available for the ADSP-BF70x EZ-Board:


Camera EI3 Extender Board

WVGA/LCD EI3 Extender Board

Audio EI3 Extender Board

Video Decoder EI3 Extender Board

Video Encoder EI3 Extender Board


A Board Support Package is available for each EZ-Extender board, which includes examples for all on-chip and off-chip drivers.


  • Additional Hardware

The ADZS-BF707 Blackfin Low-power Imaging Platform (BLIP) evaluation hardware provides a low-cost hardware solution for evaluating vision platform targeting a vast array of real-time sensing applications.


The ADSP-BF706 EZ-Kit Lite mini evaluation hardware provides an ultra low-power, low-cost hardware solution for evaluating the ADSP-BF70x Blackfin+ processor family.



What other resources are available to help with my evaluation?



ADSP-BF70x Hardware Reference Manual

ADSP-BF707 EZ-KIT manual


  • Examples and Sketches

The ADSP-BF70x EZ-Board Support Package and CCES include a number of code sketches and examples, a list of which can be found by going to CCES Help->Browse Examples. Code sketches are small code fragments, which can be generated with parameterized input provided by the user in CrossCore Embedded Studio. The resulting code can then be copied and pasted into a project.


The examples include Device Driver and System Services examples for a variety of peripherals and the Power-On Self Test demo, which tests the many peripherals of the ADSP-BF707 EZ-Board and is pre-programmed on the EZ-KIT during production.


A list of examples included in all Blackfin BSPs and middleware products can be found here.


  • Online Training Modules

A number of training modules are available for CrossCore Embedded Studio:



How do I contact technical support?


  • Questions about the ADSP-BF70x processor architecture, peripherals, programming, applications and hardware design, can be posted to the ADSP-BF70x Processors community.
  • Questions specific to evaluation hardware should be posted to the Hardware Tools community.
  • Questions about CCES and Add-Ins should be posted in the CrossCore Embedded Studio and Add-Ins community.
  • Email support is also available for these topics, here.