What is the difference between ADSP-21371KSWZ-2A and ADSP-21371KSWZ-2B

Document created by svander Employee on Jul 9, 2009Last modified by AndyR on Mar 17, 2011
Version 2Show Document
  • View in full screen mode

Q:


The ADSP-21371 in commercial temperature grade has two part numbers, one with suffix -2A and another with suffix -2B.  What are the differences between the two parts?

 

---------

 

A:

On the ADSP-21371 there are no audio algorithms in ROM, just the coefficients. The -2B part of the ADSP-21371 contains no ROM and the -2A contains the audio decoder coefficients. The part with the -2A suffix (ROM coefficients) requires a license.

Attachments

    Outcomes