FAQ: ADIS16375 Start-up Currents

Document created by NevadaMark Employee on Feb 4, 2014
Version 1Show Document
  • View in full screen mode

Q:

Do you have any more details on the 1.5A surge current that the ADIS16375 draws during start-up?

A:

-----------------------------------------------------------------------------------------------------------------------------------------------

At approximately 180ms, after the VDD voltage reaches 3.0V, the device will demand a short-term burst of energy that will last for ~400uS and require a peak current of 1.5A for a portion of this time. The current transient observed during device characterization is in the following picture:

FAQ-375-Start-up-Currents.PNG

Attachments

    Outcomes