Advantiv™ EVAL-ADV7625-SMZ Video Evaluation Board

Document created by mattp Employee on Jan 20, 2014Last modified by mattp Employee on Apr 19, 2017
Version 20Show Document
  • View in full screen mode

This FAQ applies to EVAL-ADV7625-SMZ.  All support files in their latest versions will be attached below.

 

Below are the support files for these evaluation board. We recommend that, if you download and use these files, you subscribe to email notifications for either the entire forum or at least this FAQ by clicking on the menu to the right.  In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.

 

UG-603User Guide for this evaluation board
EVAL-ADV7625-SMZ_rev0p1_schems_20150811.pdf

Schematics (in PDF format) for this evaluation board

EVAL-ADV7625-SMZ_rev0p1_schems_OrCAD_20150811.zipSchematics (in OrCAD format) for this evaluation board.
AVES3_EVAL-ADV7625-SMZ_20160127.zipAVES3 folder for this evaluation board
EVAL-ADV7625-SMZ_BOM_20140911.pdfBOM for this evaluation board
EVAL-ADV7625-SMZ_Allegro_layout_rev_0p1_20140730.zipLayout (in Allegro format) for this evaluation board
BF_7625_XREP_X2.4_REL_20160425.bin

Application binary for EVAL-ADV7625-SMZ which will configure the ADV7625 to behave like an ADV7625. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide. Note: This loader file is in binary format in order to be compatible with u-boot.

BF_7626_XREP_X2.4_REL_20160425.bin

Application binary for EVAL-ADV7625-SMZ which will configure the ADV7625 to behave like an ADV7626. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide. Note: This loader file is in binary format in order to be compatible with u-boot.

BF_7627_XREP_X2.4_REL_20160425.binApplication binary for EVAL-ADV7625-SMZ which will configure the ADV7625 to behave like an ADV7627. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide. Note: This loader file is in binary format in order to be compatible with u-boot.
BF_7625_XREP_X2.2.2REL_20140625_System_Commands.pdfList of commands for BF_7625_XREP_X2.2.2REL_20140625.bin
BF_7627_XREP_X2.2.2REL_20140625_System_Commands.pdfList of commands for BF_7627_XREP_X2.2.2REL_20140625.bin
Software package source code for eval board

Download HPM software package for ADV7625 evaluation board here.

 

For documentation on software, go to ADV7625 ADV7626 ADV7627 evaluation board software package documents

Visual DSP Project

This is VDSP project file for BF_7625_7625_X2.3.3REL_20150323 software. The software folder is just empty. You can paste the Software under ADV7625_SW folder inside the VDSP Project file. Please refer document ADV7625 ADV7626 ADV7627 evaluation board software package documents Advantiv_CrossPoint_Application_Userguide_Pr1.5.pdf Appendix for the guidelines to compile the VDSP Project

Outcomes