[#5895] prepare_target_solibs in toolchain-regtest fail to check the libs

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#5895] prepare_target_solibs in toolchain-regtest fail to check the libs

Submitted By: Mingquan Pan

Open Date

2010-02-11 00:29:56     Close Date

2010-02-11 21:40:41

Priority:

Medium     Assignee:

Nobody

Board:

N/A     Silicon Revision:

Resolution:

N/A     Fixed In Release:

N/A

Processor:

BF537     

Host Operating System:

toolchain rev.:

trunk head 4.3     kernel rev.:

State:

Closed     Found In Release:

2010R1

Is this bug repeatable?:

N/A     

Summary: prepare_target_solibs in toolchain-regtest fail to check the libs

Details:

 

prepare_target_solibs in toolchain-regtest fail to check the libs.

 

test@41-bf537-toolchain:~/work/cruise/checkouts/toolchain/buildscript> ./toolchain-regtest -s /home/test/work/cruise/checkouts/toolchain -o /home//test//work//cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Feb_10_12_27/bfin -b /home/test/work/cruise/temp0211/regtest_build43 -t linux-uclibc -T 10.100.4.50  -L

Targets: linux-uclibc

Components: binutils gas ld gdb gcc g++ gfortran objc libstdc++ libmudflap libgomp newlib

Host: i686-pc-linux-gnu

Build: i686-pc-linux-gnu

Found multiple versions of runtest, using the one at /usr/bin/runtest

Found multiple versions of bc, using the one at /usr/bin/bc

Found multiple versions of killall, using the one at /usr/bin/killall

Found multiple versions of pstree, using the one at /usr/bin/pstree

Found multiple versions of rsh, using the one at /usr/bin/rsh

Found multiple versions of rcp, using the one at /usr/bin/rcp

Toolchain source is at      /home/test/work/cruise/checkouts/toolchain

Build will be done in       /home/test/work/cruise/temp0211/regtest_build43

Path for test results

  linux-uclibc (10.100.4.50):  /home/test/work/cruise/temp0211/regtest_build43/tests/hardware-fdpic

Creating log file           /home/test/work/cruise/temp0211/regtest_build43/logs/regtest.log

rcp: /gdbserver: Permission denied

    checking host   /proc/sys/net/ipv4/tcp_tw_recycle : 1 - looks OK

    checking target /proc/sys/net/ipv4/tcp_tw_recycle : 1 - looks OK

    Target 10.100.4.50 is bf537-0.2, using that for testing multilib

    Looks like flat userspace - I'll check /lib/*.so are the same when testing

Setting up site.exp

*** Testing linux-uclibc on hw                      Thu Feb 11 12:59:46 CST 2010

GCC version                 4.3.4

GCC                         /home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Feb_10_12_27/bfin-linux-uclibc/bin

*** Checking shared libraries on target             Thu Feb 11 12:59:47 CST 2010

/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Feb_10_12_27/bfin-linux-uclibc/bin/../bfin-linux-uclibc/runtime/usr/lib/../../lib/ld-uClibc-0.9.29.so\n

md5sum: can't open '/lib/ld-uClibc-0.9.29.so': No such file or directory

 

Libs on board are different, aborting tests

specifically ld-uClibc-0.9.29.so and /home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Feb_10_12_27/bfin-linux-uclibc/bin/../bfin-linux-uclibc/runtime/usr/lib/../../lib/ld-uClibc-0.9.29.so

 

 

on the target board, there are:

root:/> ls lib/

ld-uClibc.so.0     libgfortran.so.3   libnsl.so.0        libstdc++.so.6

libc.so.0          libgomp.so.1       libobjc.so.2       libthread_db.so.1

libcrypt.so.0      libm.so.0          libpthread.so.0    libutil.so.0

libdl.so.0         libmudflap.so.0    libresolv.so.0     modules

libgcc_s.so.1      libmudflapth.so.0  librt.so.0

root:/>

 

And no detailed libs there.

 

Follow-ups

 

--- Mingquan Pan                                             2010-02-11 21:40:03

Add a -c option to use this function when needed.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes