[#6089] test gcc.dg/cpp/_Pragma6.c fail with bfin-elf

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#6089] test gcc.dg/cpp/_Pragma6.c fail with bfin-elf

Submitted By: Vivi Li

Open Date

2010-07-02 02:34:36     Close Date

2010-07-07 01:25:23

Priority:

Medium High     Assignee:

David Gibson

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2010R1

Is this bug repeatable?:

N/A     

Summary: test gcc.dg/cpp/_Pragma6.c fail with bfin-elf

Details:

 

test gcc.dg/cpp/_Pragma6.c fail with bfin-elf.

Due to its warning, maybe gcc testsuites need to modify.

 

This is new since toolchain svn version 4671.

 

--

Executing on host: bfin-elf-gcc /home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.dg/cpp/_Pragma6.c    -ansi -pedantic-errors -fno-show-column -S  -msim  -o _Pragma6.s    (timeout = 300)

spawn bfin-elf-gcc /home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.dg/cpp/_Pragma6.c -ansi -pedantic-errors -fno-show-column -S -msim -o _Pragma6.s

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.dg/cpp/_Pragma6.c:9: warning: #pragma pack(push[, id], <n>) is not supported on this target

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.dg/cpp/_Pragma6.c:11: warning: #pragma pack(pop[, id], <n>) is not supported on this target

 

FAIL: gcc.dg/cpp/_Pragma6.c (test for excess errors)

--

 

Follow-ups

 

--- David Gibson                                             2010-07-05 06:46:38

The test is for a compiler feature unsupported in the current gcc compilers for

blackfin (Pragma pack, enabled by the GCC feature macros

HANDLE_PRAGMA_PACK_PUSH_POP and HANDLE_PRAGMA_PACK_WITH_EXPANSION).

Checking in a change to the testcase so it is avoided in future.

I'm not sure how this passed in the past.

Vivi, do you have a log transcript for a testrun prior to revision 4671? So we

can see the previous behaviour?

Thanks,

D.

 

--- Vivi Li                                                  2010-07-05 23:51:05

I recheck the log and this should be always fail in gcc4.3.

I switched some regression machine which was still testing gcc 4.1 to 4.3 on

Jun 28. So please ignore revision 4671 in my latest reported bug.

I will clear the log on regression and update these bugs.

 

--- Vivi Li                                                  2010-07-07 01:25:23

This test is now marked "UNSUPPORTED".

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes