[#6234] No rpm package for full uclibc in 2010R1-rc1

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#6234] No rpm package for full uclibc in 2010R1-rc1

Submitted By: Vivi Li

Open Date

2010-09-02 23:58:44     Close Date

2010-09-13 23:19:34


Medium High     Assignee:

Vivi Li

Stuart Henderson


N/A     Silicon Revision:


Fixed     Fixed In Release:




Host Operating System:

toolchain rev.:

    kernel rev.:


Closed     Found In Release:


Is this bug repeatable?:


Summary: No rpm package for full uclibc in 2010R1-rc1



No rpm package for full uclibc and jtag tools in 2010R1-rc1.

In 09r1.1 release, we have blackfin-jtag-tools-09r1.1-2.i386.rpm and blackfin-toolchain-uclibc-full-09r1.1-1.i386.rpm.




--- Mike Frysinger                                           2010-09-03 00:11:25

the jtag tools are part of the standard rpms now.  there is no separate pkg.


as for the full uclibc, i'm not sure we're going to do one this release.


--- Vivi Li                                                  2010-09-03 02:27:35

I can't find bfin-jtag after rpms are installed.



ls /opt/uClinux/bfin-*/bin*


bfin-elf-addr2line  bfin-elf-c++filt  bfin-elf-g++-4.3.5  bfin-elf-gdb    

bfin-elf-ld.real  bfin-elf-readelf

bfin-elf-ar         bfin-elf-cpp      bfin-elf-gcc        bfin-elf-gdbtui 

bfin-elf-nm       bfin-elf-run

bfin-elf-as         bfin-elf-elf2flt  bfin-elf-gcc-4.3.5  bfin-elf-insight

bfin-elf-objcopy  bfin-elf-size

bfin-elf-c++        bfin-elf-flthdr   bfin-elf-gccbug     bfin-elf-ld     

bfin-elf-objdump  bfin-elf-strings

bfin-elf-c++-4.3.5  bfin-elf-g++      bfin-elf-gcov       bfin-elf-ldr    

bfin-elf-ranlib   bfin-elf-strip



bfin-linux-uclibc-addr2line  bfin-linux-uclibc-gcc           

bfin-linux-uclibc-insight   bfin-linux-uclibc-ranlib

bfin-linux-uclibc-ar         bfin-linux-uclibc-gcc-4.3.5     

bfin-linux-uclibc-ld        bfin-linux-uclibc-readelf

bfin-linux-uclibc-as         bfin-linux-uclibc-gccbug        

bfin-linux-uclibc-ldconfig  bfin-linux-uclibc-run

bfin-linux-uclibc-c++        bfin-linux-uclibc-gcov          

bfin-linux-uclibc-ldd       bfin-linux-uclibc-size

bfin-linux-uclibc-c++-4.3.5  bfin-linux-uclibc-gdb           

bfin-linux-uclibc-ldr       bfin-linux-uclibc-strings

bfin-linux-uclibc-c++filt    bfin-linux-uclibc-gdbtui        

bfin-linux-uclibc-mkimage   bfin-linux-uclibc-strip

bfin-linux-uclibc-cpp        bfin-linux-uclibc-gen_eth_addr  


bfin-linux-uclibc-g++        bfin-linux-uclibc-gfortran      


bfin-linux-uclibc-g++-4.3.5  bfin-linux-uclibc-gfortran-4.3.5




bfin-uclinux-addr2line  bfin-uclinux-elf2flt    bfin-uclinux-gcov          

bfin-uclinux-ld       bfin-uclinux-ranlib

bfin-uclinux-ar         bfin-uclinux-flthdr     bfin-uclinux-gdb           

bfin-uclinux-ldr      bfin-uclinux-readelf

bfin-uclinux-as         bfin-uclinux-g++        bfin-uclinux-gdbtui        

bfin-uclinux-ld.real  bfin-uclinux-run

bfin-uclinux-c++        bfin-uclinux-g++-4.3.5  bfin-uclinux-gen_eth_addr  

bfin-uclinux-mkimage  bfin-uclinux-size

bfin-uclinux-c++-4.3.5  bfin-uclinux-gcc        bfin-uclinux-gfortran      

bfin-uclinux-nm       bfin-uclinux-strings

bfin-uclinux-c++filt    bfin-uclinux-gcc-4.3.5  bfin-uclinux-gfortran-4.3.5

bfin-uclinux-objcopy  bfin-uclinux-strip

bfin-uclinux-cpp        bfin-uclinux-gccbug     bfin-uclinux-insight       




--- Mike Frysinger                                           2010-09-03 18:48:28

hmm, stuart should have been getting an error during the build.  but he didnt

mention anything.


at any rate, ive added the jtag binaries in the bin dir to the rpm spec.


--- Sonic Zhang                                              2010-09-06 00:17:01

Hi Mike,

Why we don't release the full uclibc for 2010R1? We used to include it in

former releases.


--- Stuart Henderson                                         2010-09-07 04:27:39

Mike- i'm not seeing any errors during the build process.  what do you expect me

to see?


i'll try out the fix today.


--- Mike Frysinger                                           2010-09-08 03:38:12

hmm, actually i recall hitting this with Bernd before.  older versions of rpm

(like the one in the suse chroot) do not complain about unclaimed files while

newer versions (like the ones in a debian system) do.  so you wouldnt see the



ive updated the specs and such and jtag building works for me.  but you'll need

to update the flex in your chroot too ... i'll post an updated chroot tarball to

the website for it.


Sonic: if we want to do a full-uclibc, i'll have to spend (more) time getting

the spec updated.  doesnt matter to me either way.


--- Stuart Henderson                                         2010-09-08 05:25:11

Mike, since we're not using the chroot tarball, i'll update flex myself.

Presumably this should just be the latest release (2.5.35)?


--- Mike Frysinger                                           2010-09-08 11:24:47



--- Mike Frysinger                                           2010-09-08 13:32:17

ive updated the uclibc-full spec in trunk, and it seems to work for me


--- Stuart Henderson                                         2010-09-13 04:32:21

i've tried building using Mike's updated spec and it looks fine now.


--- Vivi Li                                                  2010-09-13 23:19:34

OK. Close it.












File Name     File Type     File Size     Posted By

No Files Were Found